News Releases
FOR IMMEDIATE RELEASE No. 3354
TOKYO, May 20, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that on May 21 it will launch its MELFA ASSISTA series of robots that work collaboratively with humans based on safety features such as collision detection and strict compliance with the international safety and robotic standards ISO 10218-1 and ISO/TS15066. The series also will introduce an intuitive engineering software, RT VisualBox, for quick, easy system deployment. Customers will use MELFA ASSISTA and RT VisualBox to realize more efficient production, reduce the total cost of ownership (TCO) of robotic manufacturing systems, and meet new needs for adequate distancing of workers in manufacturing sites.
MELFA ASSISTA Series collaborative robot
RT VisualBox robot engineering software
Product | Model | Specification | Release | Yearly Sales Target |
---|---|---|---|---|
MELFA ASSISTA Collaborative Robot | RV-5AS-D | 5kg load capacity and 6-axis movement | May 21, 2020 | 1,000 units |
RT VisualBox Engineering Software | 3G-30C-WINJ/E | Windows 10 compatible | 1,000 sets |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.