Products & Solutions

Semiconductors & Devices

Mitsubishi Electric provides semiconductors/devices including power modules and high power devices that handle the highly efficient control of power, optical devices that deliver the performance required in fibre-optic communication devices, high frequency devices that cover everything from radios and mobile phones to satellite communications.

Product Line-up

Power Modules

Power Modules

Mitsubishi Electric power modules are manufactured with state-of-the-art technologies that ensure the highest levels of performance and reliability while offering impressive energy savings for the products and systems they're used in. Our line-up of products is extensive, ranging from power modules developed to control high-voltage power generation, industrial manufacturing and railway systems to applications in home products, such as controlling the electricity used by air conditioners, washing machines and refrigerators. To maintain our market-leading position, the company's R&D activities aiming to realise further reductions in power consumption and size are ongoing.

  • SiC power modules
  • SOPIPM™
  • DIPIPM™
  • IPM
  • IGBT modules
  • HVIGBT modules/HVIPM
  • Power MOSFET modules
  • Diode modules
  • PFC modules

High-Power Devices

High-Power Devices

High-power devices contribute to increased efficiency and energy savings by supporting the high-voltage, high-current and usage environment of rollers in steel works, electric power systems and the subway. From rectifier diodes to a variety of Thyristors and stacks, Mitsubishi Electric offers a broad range of new high power devices.

  • Rectifier Diodes
  • Thyristors

Driver IC

Mitsubishi Electric’s lineup of power semiconductors includes HVICs (High Voltage IC). An HVIC is a high-voltage IC with various built-in protection functions; it uses input signals from a microcomputer or other device to directly drive gates in power MOSFETs or IGBTs.

  • HVICs (High Voltage IC)

High-Frequency Devices

High-Frequency Devices

Mitsubishi Electric has long supported the advancement of wireless communication networks through the development of its high frequency devices. Products manufactured utilising the latest electronics and other technologies combined with newly developed high-performance materials have kept us in a market leading position. Our range of high-frequency devices are contributing to the wireless communications infrastructure, helping achieve more reliable wireless communications such as satellite communications, as well as smaller and more powerful mobile phones, and other high-performance network equipment.

  • GaN High-Frequency Devices
  • GaAs High-Frequency Devices
  • Silicon RF Devices

Optical Devices

Optical Devices

Mitsubishi Electric is at the forefront of industry in the development and production of laser diode products as used in modern fiber-to-the-home (FTTH) networks, 5G mobile networks and datacenters.
Further to this the lineup covers laser diode products for display and industrial applications. Our mass-produced laser diodes are renowned for its energy savings, reliability and high performance.

  • Optical Fibre Communication Devices
  • Laser Diodes for Industry & Display

Contact Image Sensors

Contact Image Sensors

With a highly-sensitive and high-S/N CMOS image sensor and an ASIC that incorporates a dedicated image processing unit and a high-precision A/D converter, Mitsubishi Electric's Contact Image Sensors deliver the world's fastest scanning speed in its class and digital output for maximum usability.


For more information