FOR IMMEDIATE RELEASE No. 3132
High output power and low distortion will help downsize satellite earth stations
TOKYO, October 4, 2017 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it will launch a Ka-band (26-40GHz) 8W gallium nitride (GaN) high-electron mobility transistor (HEMT) monolithic microwave integrated circuit (MMIC) amplifier for satellite earth stations. The new MGFG5H3001, which offers industry top-level low distortion and output power rating of 8W, boasts a small footprint that will help to downsize power transmitters. Mitsubishi Electric will begin shipping samples on November 1.
Ka-band GaN-HEMT MMIC (MGFG5H3001)
Satellite networks, which are used for high-speed communication during natural disasters and in areas where ground networks are difficult to construct, are currently implemented mainly in the C-band (4-8GHz) and Ku-band (12-18GHz), but higher frequencies are increasingly being used. Also, market demands for deployments in the higher-frequency Ka-band are increasing. Mitsubishi Electric's new Ka-band GaN-HEMT MMIC will help meet the growing demand for higher frequency deployments, as well as facilitate the development of satellite communications equipment capable of extra-high output power and efficiency.
Product | Application | Model | Overview | Shipment | ||
---|---|---|---|---|---|---|
Frequency | Saturated output power |
Linear gain |
||||
Ka-band GaN-HEMT MMIC |
Satellite earth stations |
MGFG5H3001 | 27.5-31.0GHz | 39.0dBm (8W) |
15.0dB | Nov. 1, 2017 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.