FOR IMMEDIATE RELEASE No. 2958
Achieves market-leading vibration resistance and operating temperature range
TOKYO, September 16, 2015 – Mitsubishi Electric Corporation announced today the coming launch of a new Tough Series 10.4-inch XGA TFT-LCD module for industrial applications such as construction, agricultural vehicles, factory automation and weaving equipment. The module offers 6.8G vibration-resistant acceleration seven times greater than that of conventional modules, as well as an operating temperature range of -40 to 85 degrees Celsius, 1,200cd/m2 super-high brightness and high contrast ratios. Sample sales will begin October 1 through Mitsubishi Electric offices worldwide.
Mitsubishi Electric Color Tough Series TFT-LCD module
AT104XH11
The new Tough Series TFT-LCD module meets increasing market demands for resistance to extreme temperatures and strong vibrations for versatile applications and installations.
Product | Model | Brightness (cd/m2) |
Shipment |
Tough Series 10.4-inch XGA TFT-LCD Module |
AT104XH11 | 1200 | October 1, 2015 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.