FOR IMMEDIATE RELEASE No. 3037
Will contribute to faster transmission rates in outdoor mobile communication equipment
TOKYO, July 20, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping a 25Gbps distributed feedback (DFB) laser diode for optical transmission between base stations and central offices in radio access networks within mobile telecommunication systems on September 1.
25Gbps DFB laser diode (ML764AA58T)
Communication equipment transceivers for next-generation mobile networks must support 25Gbps transmissions, wide-ranging outdoor weather conditions and compactness. In response, Mitsubishi Electric's new TO-CAN DFB laser offers 25Gbps modulation, an industry-leading operating temperature range of -20 degrees Celsius to 85 degrees Celsius and a package size that meets the SFP28 standard for 25Gbps compact transceivers.
Product | Model | Feature | Shipment date |
---|---|---|---|
25Gbps DFB laser diode | ML764AA58T | -1310nm wavelength -φ5.6mm TO-CAN Package |
September 1, 2016 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.