FOR IMMEDIATE RELEASE No. 3029
First MOSFET module to offer automatic mounting on printed circuit boards of professional transceivers
TOKYO, June 15, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will commercially launch new silicon radio-frequency (RF) high-output metal-oxide-semiconductor field-effect transistor (MOSFET) modules capable of automatic mounting on printed circuit boards of professional radio equipment on July 1. As the first MOSFET models in the 60W-output class to offer this capability (according to Mitsubishi's own research as of June 15), the modules are expected to raise the productivity of professional radio equipment manufacturing by eliminating the need for screws and other mounting processes. Two types of modules providing the transmitter circuitry of professional transceiver equipment will be available as a pair.
Silicon RF high-output MOSFET module pair
High-power amps for professional radio equipment commonly are mounted on their cabinets with screws, which has prompted calls for more efficient mounting solutions. In addition to responding to this need, Mitsubishi Electric's new MOSFET modules will help reduce to the size and power consumption of radio equipment.
Operating frequency |
Model* | Specification | Shipment | |||
---|---|---|---|---|---|---|
Operating voltage |
Input power |
Output power |
Power efficiency |
|||
135-175MHz | RA05H1317MS1 | 12.5V | 10mW | 85W | 60% | July 1st |
RA60H1317MS1 | ||||||
378-470MHz | RA05H3353MS1 | 53% | ||||
RA60H3847MS1 | ||||||
440-527MHz | RA05H3353MS1 | 52% | ||||
RA60H4453MS1 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.