FOR IMMEDIATE RELEASE No. 3016
17 new models will better meet demand for low power loss, highly reliable industrial equipment
TOKYO, March 30, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it would begin shipping samples of 17 new models of T series power semiconductor modules featuring seventh-generation insulated-gate bipolar transistors (IGBTs). The new modules have a 1.7kV rating and realize improved power loss and reliability for general-purpose inverters, uninterruptible power supplies (UPS), photovoltaic (PV), wind power-generation systems and other industrial equipment. Sample shipments will begin September 30.
The modules will be exhibited at major trade shows including MOTORTECH JAPAN 2016 during TECHNO-FRONTIER 2016 in Japan from April 20 to 22, Power Conversion Intelligent Motion (PCIM) Europe 2016 in Nuremberg, Germany, from May 10 to 12, and PCIM Asia 2016 in Shanghai, China, from June 28 to 30.
NX-type Solder Pin Package
NX-type Press Fit Pin Package
Standard-type Package
Package | Voltage Rating | Current Rating | Shipment |
---|---|---|---|
NX-type Solder Pin Package |
1.7kV | 100, 150, 225, 300, 450, 600A | From September 30 |
NX-type Press Fit Pin Package |
100, 150, 225, 300, 450, 600A | ||
Standard-type Package |
75, 100, 150, 200, 300A |
Note that the releases are accurate at the time of publication but may be subject to change without notice.