News Releases

Mitsubishi Electric to Launch LV100-type T-series IGBT Module for Industrial Use

Will reduce power consumption and size of renewable-energy power-supply systems, and more

FOR IMMEDIATE RELEASE No. 3367

TOKYO, August 25, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of its LV100-type T-series insulated-gate bipolar transistor (IGBT) module for industrial uses. The LV100 package, which achieves high versatility and high current density, has been used widely in railway and electric power applications and now has been adapted for industrial uses. It is expected to help reduce the size and power loss of power converters, specifically inverters used for renewable energy applications such as photovoltaic and wind-power generation, and also high-capacity motor drives. Sales will start this September.

LV100-type T-series IGBT module for industrial use

Product Features

  1. 1)Common-outline LV100 package adapted and optimized for industrial uses
    • The LV100 package, used widely in railway and electric power applications, has been adapted and optimized to help standardize packages for industrial applications.
  2. 2)Industry-leading current density for small and more power-efficient inverters
    • The LV100 is equipped with the latest (7th-generation) IGBT, which uses the CSTBT™ 1 structure, and RFC (Relax Field of Cathode) diode2 for low power loss. Industry-leading3 current density of 17.14A/cm2 is realized in this high-power IGBT module by optimizing the package structure. The package will help to miniaturize power converters, such as inverters for renewable energy power sources, and high-capacity motor drives (1700V/1200A and 1200V/1200A).
    1. 1Mitsubishi Electric's original IGBT structure using the carrier storage effect
    2. 2Mitsubishi Electric's original diode that optimizes electron mobility on the cathode side
    3. 3As of August 25, 2020 according to Mitsubishi Electric research
  3. 3)Optimized internal structure for more reliable inverter systems
    • Integrating the insulated and copper-base parts in the structure, and optimizing the internal electrode structure, increases thermal cycle life4 and achieves the industry's highest-class3 low-package inductance, which will contribute to equipment reliability.
    • The terminal layout is optimized for easy paralleling and flexible inverter configurations and capacities.
    • Three AC main terminals help to spread and equalize current density for increased inverter capacity.
    1. 4Lifespan due to stress-strain caused by relatively gradual temperature change generated by system start and stop

Sales Schedule

Product Model Rating Release date
LV100-type T-series
IGBT module for industrial use
CM800DW-24T 1200V / 800A September 2020
CM1200DW-24T 1200V / 1200A
CM800DW-34T 1700V / 800A
CM800DW-34TA5 1700V / 800A
CM1200DW-34T 1700V / 1200A
  1. 5CM800DW-34TA uses a large free-wheeling diode

Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.


Inquiry

Media contact

Customer Inquiries